Comunicados de imprensa

A mostrar 31 - 40 de 64 resultados encontrados
22/01/2018

Armstrong Fluid Technology has announced the availability of a new line of high performance Design Envelope End-Suction pumps in the 1 to 10 hp range. These new offerings reflect a completely new design featuring improved hydraulics and Armstrong intelligent motor technology. The new offerings also feature Armstrong’s unique vibration isolation technology, which can reduce installed costs by as much as $2000 by eliminating the need to add an inertia base on installation.

22/01/2018

Armstrong Fluid Technology has announced a new Performance Management Service offering, available with the purchase of all new Design Envelope pumps. This new service is being offered on a free trial basis ending in December 2018. Owners and end users can sign up for the introductory offer as an integral part of the warranty registration.

18/01/2018

Armstrong Fluid Technology has announced the availability of its next-level of innovation in Design Envelope pumping solutions across the entire pump range.

18/01/2018

As part of its global sustainability initiative, Armstrong Fluid Technology has helped customers worldwide save more than one billion kWh of electricity with an estimated value of over $100 million since 2007. These energy savings averted nearly 350 tons of CO2 emissions, which is equivalent to taking 75,000 cars off the road for one year.

18/01/2018

Armstrong Fluid Technology has announced a new service that will provide up to 25% savings compared to traditional variable speed plant operation.

08/01/2018

Armstrong Fluid Technology announces that it has completed the acquisition of the Circulator Pump Business Unit of HALM Motors + Systems GmbH in Germany, a provider of high efficiency circulator pumps for heating, solar, geothermal and domestic hot water applications.

14/06/2017

Armstrong Fluid Technology has announced a new address for its Shanghai office, which will now serve as both a Regional Sales Excellence Center and headquarters for the company’s operations in China and Asia Pacific.

11/06/2017

Armstrong Fluid Technology announced that its recently introduced line of Design Envelope Generation 5 pumps now meet the IE5 efficiency standard for motors. This includes the new Design Envelope TangoTM parallel pumps and Design Envelope Vertical In-Line pumps up to 10hp.

14/04/2017

Armstrong Fluid Technology has enhanced its Fireset™ Horizontal Split Case (HSC) pump line with two new technologically advanced models.

10/03/2017

Armstrong Fluid Technology announced that its employees have donated $10,000 to WaterAid, an international charity dedicated to providing access to safe water, hygiene and sanitation worldwide.

A mostrar 31 - 40 de 64 resultados encontrados

Kits de peças genuínas Armstrong

Todas as peças de que necessita para manter os seus sistemas a funcionar na perfeição.

Encontrar um kit de peças

recursos & ferramentas

Dispomos de uma variedade de materiais e ferramentas de apoio online gratuito. Encontre os elementos essenciais para aprender, aplicar e efetuar a manutenção do equipamento Armstrong.

Iniciar

Entre em contato

Estamos felizes por ajudar. Discuta as necessidades do seu projeto e de produtos connosco, verifique o estado dos seus envios ou permita-nos salvar o dia em caso de emergência.

Entre em contato