Armstrong In The Media

Fire Pump Types

Posted by Armstrong Fluid Technology on Apr 16, 2024 10:37:38 AM

Pumps that are designed and approved for fire suppression systems can be grouped into four major categories based on configuration.

Read More

Topics: Design Envelope, Fire Pumps

Design Envelope Fire Pump Unit

Posted by Armstrong Fluid Technology on Apr 16, 2024 10:36:03 AM

Design Envelope Fire pumps are designed, assembled, and tested to meet the code requirements of a Self-Regulating Variable Speed Fire Pump Unit, as described in NFPA 20 – 2019 edition. Design Envelope Fire pumps are factory-built, integrated fire pumps consisting of a Vertical In-Line pump, driver, and variable speed control unit. They’re configured to maintain a set pressure until the maximum power draw is reached, while modulating pump speed to control to meet limits on pressure or suction.

Read More

Topics: Design Envelope, Fire Pumps, Design Envelope Fire pump unit

Horizontal Split Case Fire Pump

Posted by Armstrong Fluid Technology on Apr 15, 2024 5:16:23 AM

Horizontal Split Case Fire Pump

 

 

These pumps use a between-the-bearings design, which means that the impeller is supported by bearings on both sides. This design provides more support for the impeller and enables it to rotate more efficiently under stress. HSC pumps place the suction and discharge nozzles (flanges) in the bottom half of the casing, on opposite sides. The impeller shaft is positioned slightly above the flanges. This sturdy but simple design is particularly suitable for higher flow applications, because it reduces thrust loads on the pump shaft and allows for operation over a broad range of flows.

Read More

Topics: Fire Pumps, Pumps

Armstrong Celebrates 90th Anniversary

Posted by Armstrong Fluid Technology on Apr 12, 2024 1:19:45 AM
As Seen On: contractormag.com April 04, 2024
 
Since its founding in 1934 the company has expanded from the challenges of the Great Depression to become a leader in its field.
 
TORONTO, CAN —   Armstrong Fluid Technology  marked its 90th anniversary this April, celebrating a significant milestone of longevity and innovation in the fluid-flow systems industry. Since its founding in Toronto, Canada, in 1934 by Samuel Allan Armstrong, the company has expanded from the challenges of the Great Depression to become a leader in its field. Today, Armstrong operates eight manufacturing facilities across four continents, showcasing its global reach and commitment to excellence in design, engineering, and manufacturing.
 
Read More

Topics: In The Media, CEO

Circuit Balancing Valves (CBVs)

Posted by Armstrong Fluid Technology on Apr 4, 2024 2:52:17 PM

Where do Circuit Balancing Valves (CBVs) fit in a hydronic system?

 CBVs should be included in every branch of a hydronic system. For many applications such as boilers, chillers and heat pumps, they are needed to ensure balanced or equalized flow of water to all parts of a building and, as required by heating or cooling loads, across all branches of a system.

Read More

Topics: Hydronics, In The Media, CBV

Data centres are feeling the heat

Posted by Armstrong Fluid Technology on Jan 29, 2024 11:17:07 PM

As Seen On: technicalreviewmiddleeast.com January 22, 2024

 

 

Packaged chiller plant rooms within data centres cut installation time by up to 95%. (Image source: Adobe Stock)

Kevin Laidler, sales director for Middle East and Africa at Armstrong Fluid Technology, writes forTechnical Review Middle East, explaining how innovations in the HVAC sector can help data centres.

Read More

Topics: Data Center, HVAC, HVAC System, In The Media, HVAC Installations

Case study: Upside Down Condos II

Posted by Armstrong Fluid Technology on Jan 2, 2024 9:30:00 AM

This condo tower (324 units on 13 floors) had completed a previous retrofit that unfortunately left the variable speed pumps operating in a fixed mode at low speed, so the HVAC system couldn’t cool the west-facing units in the summer.

Read More

Topics: Energy Saving, Energy Upgrade, Energy - saving pumps, In The Media

Case study: Central Memorial High School

Posted by Armstrong Fluid Technology on Dec 27, 2023 9:30:00 AM

Central Memorial High School creates opportunities for 1100 students to focus on the arts, athletics or trades. In 2018, Armstrong worked with the Calgary board of Education to upgrade the hvac system for better efficiency and comfort.

Read More

Topics: Energy, Energy Upgrade, Energy - saving pumps, In The Media

Case study: Commercial Towers, Toronto

Posted by Armstrong Fluid Technology on Dec 22, 2023 9:30:00 AM

A pair of commercial towers (18 floors and 24 floors) in downtown Toronto recently completed an HVAC upgrade. The owners agreed to a proposal to replace 3 constant speed 40hp pumps with new Design Envelope pumps plus Pump Manager.

Read More

Topics: Energy Saving, Energy Upgrade, Energy - saving pumps, In The Media

Case study: Crown Realty Partner: Pearson Corporate Center

Posted by Armstrong Fluid Technology on Dec 19, 2023 9:30:00 AM

Crown Realty Partners: Pearson Corporate Center is a 300,000 square foot complex in Toronto consisting of two eight-storey office towers joined together by a central atrium. In 2018 the building owners asked Armstrong to upgrade the original pumps to new Design Envelope pumps.  

Read More

Topics: Energy Saving, Energy Upgrade, Energy - saving pumps, In The Media

Never miss a thing!

Be the first to get notified

Sign up for our blog notifications and you will be one of the first to know when there is new content. If you want to be in the know, sign up now.

Sign up for notifications now

Recent Posts

Posts by Topic

see all